Industry Online Support
Technical Forum
2/27/2008 9:23 AM | |
Posts: 13 Rating: (1) |
Hi Thans for the response.I ve used AG_SEND & AG_RECV blocks after configuring in Netpro with "S7 Fault Tolerent connection".But its not working out Find attached the configuration which I did. Anticipating fast response at earliest. Thanks in adnvance. Regards SKR AttachmentEthern_1.zip (315 Downloads) |
2/28/2008 1:34 PM | |
Posts: 5822 Rating: (412)
|
Dear SKR, if the following documents do not help not even I can help you: How do you program communication blocks FB12 "BSEND" and FB13 "BRCV" for data exchange on the S7-300? Just be aware that the BSEND / BRCV Functions on the S7-400 are SFBs, not FBs. S7 Communication with BSEND/BRECEIVE via PROFIBUS CPs PROFIBUS behaves just like Ethernet so no problem. Programming an S7 Communication between two CPU modules for STEP 7 and CFC Best regards J_Bell |
Last edited by: J_Bell at: 28.02.2008 13:36 |
|
3/4/2008 9:51 AM | |
Posts: 13 Rating: (1) |
Dear Bell Thanks a lot for all your support. I ll try with these blocks and will give you the feedback. regards SKR |
Follow us on