6/12/2006 1:55 PM | |
Posts: 3149 Rating: (171)
|
Have you already checked whether/why this signal is coming from your M7??? WinCC is just displaying the arriving messages.... |
6/13/2006 8:46 AM | |
Posts: 3149 Rating: (171)
|
Hi, I must admit, that I am too young for M7. [:D] Which block/module in your M7 is generating these messages??? => try to switch the module e.g. off nemo |
6/15/2006 12:22 PM | |
Posts: 32 Rating: (0) |
Anybody has any suggest for me. |
6/21/2006 4:05 AM | |
Posts: 32 Rating: (0) |
Dear Salma, Here is exported file from Alarm Logging Pls, see and give me your suggest. Best regards, SmallMonkey |
6/21/2006 4:08 AM | |
Posts: 32 Rating: (0) |
it's difficult for attching a file.AttachmentAlarmLogging.zip (283 Downloads) |
6/21/2006 4:12 AM | |
Posts: 32 Rating: (0) |
here is some pictures that was captured from screen. SmallMonkey |
6/21/2006 9:34 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (151)
|
Thanks for posting your data here. OK. In WinCC, each alarm must be triggered by a separate tag. Your system is using one tag to trigger and acknowledge ALL alarms.You are using the SICAMM7.nll file to process the alarms which means that you are not using a standard WinCC alarm configuration. My guess that it is something it this file that is causing the problem and not WinCC. Unfortunately I know nothing about SICAM so I cannot help. I would recommend that you contact the hotline (using the Support Requestlink) if no-one else on this forum can help. |
Follow us on