8/12/2021 2:42 AM | |
Joined: 10/13/2008 Last visit: 11/11/2022 Posts: 41 Rating: (2) |
Hello, can you help specify the exact location of the smileytool in PCS7 V9.0 SP2, thank you! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/12/2021 09:08:48New subject after splitting |
|
8/12/2021 6:30 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi, You post a great quiz question. I think you mean the parameter interface in SIMATIC BATCH where you can set parameters as source or destination? If so, you can find it under Parameters tab when pressing the more button on the right side of the parameter, you get a expanded list where you can select the parameter as source or destination in one of the rows. If not, please specify your quiz question |
If I could help you, you can use the RATE button. Thank you. |
|
8/16/2021 8:36 AM | |
Posts: 198 Rating: (60) |
Hello mhike, According to the SIMATIC BATCH COM API V9.0SP1 manual, the sample project link points to "Sample Application for SIMATIC BATCH COM API" which is available in this link: https://support.industry.siemens.com/cs/ww/en/view/92344632 As of now, there is no link to download the latest version (9.0 or 9.0.1) of the dll (Smiley tool). Also, it is not available in the path as mentioned in your old linked post. It was removed after Batch V8.2. However, from what I understand, you should be still able to use this tool (downloaded from the above link) in 9.x versions considering that it is mentioned in the manual. (though the drop down in the version restricts usage to 8.2) Hope this helps |
Follow us on