3/3/2011 2:59 AM | |
Posts: 2964 Rating: (478) |
Hello Makaveli, Give me the Feed Motor type no? Regards, Ekalavya |
3/4/2011 10:34 AM | |
Posts: 2964 Rating: (478) |
Hello, Normally NSK and NTN bearings are used on these motors.Yes it is difficult to replace the bearing on this motors at site. Whole motor need to be removed out completely…. if it is Feed motor alignment is required. I have not tried replacing bearing I have tried aligning the encoder at site it works… Regards Ekalavya AttachmentERN-1387.pdf (710 Downloads) |
Follow us on