1/20/2015 4:35 AM | |
Posts: 122 Rating: (1) |
Hello Experts, I have here a S300 CPU with the following modules 6ES7 317-2FK14-0AB0 CPU 317F -2 PN / DP 6ES7 326-1BK02-0AB0 - FDI24 * DC24V 6ES7 326-1BK02-0AB0 - FDI24 * DC24V 6ES7 326-2BF01-0AB0 - FDO10 * DC24V/2A 6ES7 323-1BL00-0AA0 - DI16 / DO16 * 24V / 0.5A 6ES7 323-1BL00-0AA0 - DI16 / DO16 * 24V / 0.5A 6ES7 323-1BL00-0AA0 - DI16 / DO16 * 24V / 0.5A 6ES7 321-1BL00-0AA0 - DI32 * DC24V. Mainly with some safety modules. I would like to program the safetly module. I haven't yet done for a siemens. Can any one write me a simple program to start with. For example, a emergency switch which would be connected to a safety module (F-Module). If this switch is switched on then the whole program has to stop or come to an end. Can any one write me a simple program using the hardware which I write here so that to enable me to understand the working of the safety module of siemens. I here with attach you also the snap shots related to my question. Looking forward to hear your response. With regards Johannes AttachmentZippedFile.zip (173 Downloads) |
Last edited by: Johannes4u at: 1/20/2015 2:48 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on