11/16/2007 9:23 AM | |
Joined: 9/11/2007 Last visit: 1/15/2009 Posts: 1 Rating: (0) |
Hello everybody, I've just installed on 3 Siemens Esprimo PC's PCS7 V7 SP1. When we create a multi-project and start the OS-RTand whenweexit the RT weget CCArchiveManager.exe has encountered a problem and needs to close. Different projects on differents PC's, same error ! Known problem ? Kind regards, Dimitri. AttachmentFault_Exit_OS_RT_PCS7_V7_SP1.zip (222 Downloads) |
11/16/2007 1:43 PM | |
Posts: 1776 Rating: (95)
|
Hi, you can check the WinCC diagnostic files and the Windows event manager See the FAQs http://support.automation.siemens.com/WW/view/en/22892165 |
1/3/2008 3:41 PM | |
Posts: 3 Rating: (0) |
I Have the same error while closing WinCC after installing PCS7 V7.0 SP1 on a SIEMENS PG. |