11/3/2011 4:07 AM | |
Posts: 19 Rating: (0) |
Dear everyone, May you help me on how to produce a current from PLC's output in range: 4-20mA ? Thank you very much for your helps. Best regards, St |
11/3/2011 6:45 AM | |
Posts: 19 Rating: (0) |
Dear Idunil, I want to program on PLC S7-300 to produce a current in range: 4 - 20mA to supply to module AFCM0000 input of Redlion (you can see in the attache files). On this module, we set range for current: 4 - 20mA, this input signal on AFCM0000 will convert to frequency (Hz or RPM) 0 - 1kHz in order for control engine speed. Example: PLC produce 4mA at AO module --------> AFCM0000 (4mA) converted to 0Hz MPU (speed sensor ) (1000RPM rotation per minute) ----------------> Engine. Thank you, Best regards AttachmentAFCM0000.pdf (331 Downloads) |
11/3/2011 7:13 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, Take a look at FC106 ( UNSCALE ) from STEP 7standard library, in the "TI-S7-Converting Blocks". And more at http://support.automation.siemens.com/WW/view/en/8859629 (from 269th page). Best regards, Hristo Mihalev |
11/3/2011 9:26 AM | |
Posts: 19 Rating: (0) |
Hi Indunil, This is the image of HW, that I post to you. Thank you |
11/3/2011 12:48 PM | |
Posts: 19 Rating: (0) |
Thank you Marcjan |
This contribution was helpful to1 thankful Users |
Follow us on