1/19/2013 9:00 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (927) |
You know about the function: Block types? Its under options->Block types while in CFC chart.. The systems removes unused blocks from Blocks folder, but also from CFC charts.. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
1/20/2013 10:41 AM | |
Posts: 14 Rating: (0) |
Yes, This function I've used for the PLC project. But it's not helping me to clean up the library as I hoped. |
1/20/2013 10:52 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (927) |
Well, still not sure you want to do here... In the library you want to delete blocks? I assume you are talking about the master library since you can create this by adding blocks to it.... Deleting the blocks from the master library will should do the trick. What are you trying to accomplish? Cant you just simply hide the libray? if that not enough? If your are talking about SCL sources you used to create your own blocks, you can A: protect them by adding the attribute: KNOW_HOW_PROTECT and B: find the default FB name where instances are created from and delete that from the Block folder. So can you explain better what you want excactly? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on