2/10/2016 4:08 PM | |
Joined: 12/28/2015 Last visit: 1/24/2024 Posts: 256 Rating: (26) |
Hello, Have you check the data types of plc and wincc and the address? |
2/10/2016 4:18 PM | |
Posts: 223 Rating: (0) |
Yes, all those things are configured like they should be. But I think it's a problem in one of my scripts... |
2/11/2016 10:03 AM | |
Posts: 223 Rating: (0) |
How can I evaluate the quality code? |
2/11/2016 1:12 PM | |
Posts: 223 Rating: (0) |
In the PLC, it's a real value. I work with an unsigned word in WinCC, so the format adaption is WordToUnsignedWord (whith which, there's no conversion) |
2/12/2016 3:06 PM | |
Posts: 223 Rating: (0) |
Ok The value is connected good now. I don't know what the problem was, but it seems to work now... |
This contribution was helpful to1 thankful Users |
7/14/2016 10:39 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by GarryT is split to a separate thread with the subject WinCC 7.2.0.8, values show zero. Best regards |
Follow us on