Industry Online Support
Technical Forum
3/18/2013 4:06 PM | |
Posts: 5 Rating: (0) |
WHICH PARAMETERS ARE REQUIRED FOR EXTERNALLY SUPPLIED DC LINK VOLTAGE-560 VDC IN 4.4 KW MM440 DRIVE,ABSENCE OF MAINS POWER. |
3/19/2013 4:42 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi vrparmar, Application for Drive Technology - Siemens |
3/19/2013 4:45 PM | |
Posts: 13 Rating: (0) |
For a DC link coupling, the VDCmax controller, integrated in the MICROMASTER 420 and MICROMASTER 440 frequency inverters may not be used. This controller is activated in the factory setting which means that it must be disabled by setting parameter P1240 to 0. Check out this document, it can help you!
AttachmentMM4App_007_DC_link_coupling_en.pdf (73 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on