1/19/2011 10:04 AM | |
Joined: 9/14/2009 Last visit: 12/7/2023 Posts: 41 Rating: (0) |
First alot thanks for you i attched diago.buffer report you asked and attched the program compressed to clear problem note the ID address is the same 80 in drive and H.W Config. Regards, AttachmentProg.and Report.zip (150 Downloads) |
1/20/2011 12:29 AM | |
Joined: 7/2/2008 Last visit: 8/26/2024 Posts: 928 Rating: (308)
|
Hello esem2704 ,
Please change your project settings before you upload it in the future. Always make it language neutral so members can open it easily. Why does a message appear indicating that a foreign language has to be installed in the operating system when a project is opened from STEP 7 version V5.3 SP2? Now back to your project, in FC34-Network 3 you can find that the input address byte 49 is used without having a peripheral in hardware configuration. Maybe you have changed a module in hardware configuration that was taking the input address 49. Best regards. H-H AttachmentS7-400.zip (153 Downloads) |
Follow us on