8/1/2011 11:53 AM | |
Posts: 3 Rating: (0) |
Hai, This is kind of problem i faced while trying to do the program transfer in the 802D, the problem was some extra charecters are getting added up in the program received (Please find the Program attached which I have received from the machine.). Since some extra characters are getting added up machine is note receiving the program back (I have remove the extra characters and then send it back but thats some thing I don't want to do). Please help me on this. Thanks in advance Attachment1000.zip (57 Downloads) |
8/1/2011 2:50 PM | |
Joined: 1/19/2008 Last visit: 4/19/2024 Posts: 980 Rating: (63) |
Hi, I think you are outputting as a binary backup file Output in punch tape format with cr Pee |
Follow us on