Industry Online Support
Technical Forum
6/11/2009 7:13 PM | |
Posts: 103 Rating: (10) |
Sydney, What is the syntax to do this? |
Last edited by: FunStuff at: 6/11/2009 7:14 PM |
|
6/12/2009 9:36 AM | |
Joined: 1/4/2008 Last visit: 2/27/2024 Posts: 703 Rating: (96) |
Hello, suppose you have a function with the input "IN_Variable" of data type POINTER. When call you assign your variable symbolically. Inside the code is to be: L P##IN_Variable LAR2 L W [AR2,P#0.0] // DB number T #w_DBnr L D [AR2,P#2.0] // bit pointer T #dw_Pointer if you want to immediately use it, then LAR2 OPN DB [#w_DBnr] L D [AR2,P#0.0] T LD 0 Regards Sydney addition: fordetailed information look to the Step7 online help for - POINTER Parameter Type - Area-Crossing Register Indirect Addressing In the attachment is description what the Address registeras well as the 32-bit pointercontains AttachmentAddress registers.pdf (337 Downloads) |
Last edited by: Sydney at: 6/12/2009 10:04 AMaddition... |
|
Follow us on