Industry Online Support
Technical Forum
5/11/2012 4:02 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477) |
What Manual is saying about this fault,
You have to check any possible short circuit on L1 phase. Remove cable, check megger value If your drive is having Safe Stop option, you can have this fault during Safe Stop operated in running condition Also There are lot of discussion regarding this Fault. You can find it using search function give on the right top corner Here are some Links but you can find more after searching F025, F026 and F027 /tf/WW/en/Posts/32964 /tf/WW/en/Posts/18373 /tf/WW/en/Posts/43903 /tf/WW/en/Posts/41892 |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to2 thankful Users |
Follow us on