11/26/2016 4:01 PM | |
Joined: 9/27/2006 Last visit: 5/9/2024 Posts: 12257 Rating: (2666)
|
Hello fizik; You can disable the pulse tests of your F-DO modules, if required. The information in the following FAQ could be of service; it was prepared for ET 200S modules, but yu should be able to extend it to your ET 200SP modules. What effect do the test pulses of fail-safe ET 200S modules have? https://support.industry.siemens.com/cs/ww/en/view/44452714 Hope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
11/30/2016 7:47 PM | |
Joined: 9/27/2006 Last visit: 5/9/2024 Posts: 12257 Rating: (2666) |
Hello fizik; A bit of search can provide many benefits on a site such as this. look for ET 200SP F-DQ modules using the Search Box on ths page, you will be amazed at what you can find: https://support.industry.siemens.com/cs/fr/en/view/78645789 See in particular the extracr included as attachment. Hope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
12/1/2016 8:28 AM | |
Joined: 2/26/2015 Last visit: 5/8/2024 Posts: 16 Rating: (0) |
Yes, the search is ama-zing! :) But ... this can only be set in TIA, as I've written in my previous post. In Step 7 v5.5 there is no such parameter .... It seems to me that nothing can be done in S7. Thanks anyway! |
12/1/2016 2:59 PM | |
Joined: 9/27/2006 Last visit: 5/9/2024 Posts: 12257 Rating: (2666) |
Hello fizik; Actually, both in TIA Portal and in Simatic manager you need an additional Safety package to parametrize any Siemens F-IO module, including the ET 200SP F-DQ: This is from the original Delivery Release information for the ET-200SP F-IO modules: https://support.industry.siemens.com/cs/ww/en/view/78618356 "Support for Configuration The new failsafe ET 200SP modules can be configured via the TIA Portal as from Safety Advanced V12 (entry ID:79206291), or with Distributed Safety V5.4 SP5 together with the S7 F-ConfigurationPack V5.5 SP11* and higher. * The delivery release of S7 F-ConfigurationPack V5.5 SP11 is planned for early November 2013." Also, from the information presented in this FAQ, you would need at least F-Confidguration Tool version 5.5 SP11 (part of Distributed Sfety package for Simatic Manager) in order to ntegrate your ET 200SP F-DQ modules: https://support.industry.siemens.com/cs/ww/en/view/15208817
Daniel Chartier |
Last edited by: dchartier at: 12/1/2016 5:23:28 PM |
|
12/14/2016 5:29 PM | |
Joined: 2/26/2015 Last visit: 5/8/2024 Posts: 16 Rating: (0) |
I received a reply from Siemens:
So, there *was* an option in the old F-CP - but is not supported anymore by the newest F-DQ/ET200SP firmware.
|
This contribution was helpful to3 thankful Users |
Follow us on