4/24/2016 4:38 PM | |
Joined: 3/17/2013 Last visit: 1/10/2021 Posts: 474 Rating:
|
Hi These F-DQ modules are used in critical Safety applications where in case of any operations abnormality safe shutdown takes place leaving EHS conditions to a safe limit. These tests are complete bit pattern tests and can be performed automatically @ a predefined time interval, to check any short or open circuits in the load connected, to determine whether operating point is shifted or any excessive current consumption of connected loads etc. If channel draws more or less current during this test it indicates by passivating the particular channel. Test procedure is attached from the part of manual you can search on web Attachmentet200sp_f-dq_4x24vdc_2a_pm_hf_manual_en-US_en-US_.pdf (264 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on