3/31/2008 8:04 PM | |
Posts: 767 Rating: (69) |
Hi all, On last friday my 417-4H redundant system was shutdown becuase of F_TESTC block caused the fail safe program shutdown. I did make the changes to the safety program on thurusday and downloaded online by deactivating the safety mode. I did activate the safty program on 5:30 on thurusday and on friday 5:30 that block caused the shutdown of safety proram means total chaos for my system. As I can see one of the reson being mentioned is the online changes in safety program can trigger that block and it run after 24 hours. Now my questions are 1) If there was any error in the safety program why it won''t come up at time of compilation. 2) If it was illegal to download those changes(fairly minor) why CPU allowed me at that time. 3) Is there anyway that I can run this F_TESTC block for test after download so that it won't happen to me again or is there is any way I can see that my online download will not cause the shutdown of safety program during the F_TESTC routine. 4) ifF_TESTC always run itself after activation of safetymode why it had not done the safety program shutdown just afteractivation of safety mode on thurusday AttachmentDiagnostic buffer.pdf (235 Downloads) |
Last edited by: Shahiiee at: 4/1/2008 9:46 AMI have attached the diagnostic buffer just look at the event numbers 233 to 228 One more thing the failsafe library version is 1.2 |
|
5/15/2008 10:39 PM | |
Posts: 2661 Rating: (279) |
For those who are still interested, the attachment contains the extract from the diagnostic buffer and the explanation why this happened. The instance DB numbers can lead to the problem blocks/instances.
AttachmentExtract from Diagnostic buffer & Explanation.pdf (249 Downloads) |
5/25/2008 2:59 PM | |
Posts: 767 Rating: (69) |
Hi, Many thanks for the reply. I investigated the matter a bit further but have not got to a result except now I don't do the changes only download. I have done changes only download so many times on this system apart from other systems but never have had any problems. As far as SFC90 is concerned for this system we never have used sfc90 in the complete project not even been added to the project also the test function time is 90 minute. AttachmentVXCcompare.zip (227 Downloads) |
Last edited by: Shahiiee at: 5/26/2008 3:21 PMLast edited by: Shahiiee at: 5/26/2008 3:18 PMLast edited by: Shahiiee at: 5/26/2008 3:15 PMLast edited by: Shahiiee at: 5/26/2008 3:14 PM |
|
5/27/2008 11:24 PM | |
Posts: 2661 Rating: (279) |
Thanks for the update. Please let us know if the tech support reports something. Regards |
Follow us on