4/28/2008 7:45 AM | |
Joined: 9/20/2006 Last visit: 3/5/2024 Posts: 307 Rating: (96) |
The value of P071 is correctly programmed. |
5/4/2017 4:34 PM | |
Posts: 2 Rating: (0) |
DEAR. Solución de la alarma F006. Se cambio el encoder que esta acoplado al eje del motor del inversor instalado en el bus DC. Este ocasiona, que se interprete como una detención del motor por lo que ocasiona que el equipo regenere. No existían alarmas en los equipos re-generativos. Nota: Archivo adjunto, equipos instalados ------------------------------------------------------------------------------------------------- DEAR. Alarm solution F006. The encoder that is coupled to the motor axis of the inverter installed on the DC bus is changed. This causes it to be interpreted as an engine stoppage causing the equipment to regenerate.
Note: Attachment, installed equipment AttachmentSolucion F06 Siemens.doc (545 Downloads) |
Last edited by: Min_Moderator at: 5/5/2017 2:22:48 PMtranslation |
|
This contribution was helpful to1 thankful Users |
5/29/2017 7:52 PM | |
Joined: 9/27/2006 Last visit: 9/21/2024 Posts: 12282 Rating: (2684) |
Hello Junior; I do not know if these were the items you already checked, but let's start with the definition of f006 from the Compendium: https://cache.industry.siemens.com/dl/files/629/109736629/att_880959/v1/vc34_kompend_e.pdf Hope ths helps, Daniel Chartier |
Follow us on