3/30/2009 12:41 PM | |
Joined: 10/18/2006 Last visit: 3/4/2022 Posts: 163 Rating: (3) |
Hi there! have you ever seen this ?? i´m attaching you this strange behaviour related to a faceplate in a OS Client ("OS_client_faceplate.JPG"). As you can see, some of the fields are displayed in gray, while in the OS Server ("OS_server_faceplate.JPG") this doesn´t happen. Is it related to the User Administrator settings? This happens with PCS7 v7.0 SP2 and the faceplate belongs to an SFC-type.
Attachmentfaceplate.zip (209 Downloads) |
3/30/2009 2:44 PM | |
Posts: 14 Rating: (0) |
But shouldn't you download from ES to OS server? The clients take data from OS server isn't it? So why transferred to os client? |
4/12/2009 7:40 AM | |
Posts: 2661 Rating: (279)
|
Please post a screenshot of the properties of the field that is grayed out. |
4/13/2009 8:13 AM | |
Posts: 69 Rating: (0) |
I don't have access to capture screen shot. Anyway, I think it doesn't help to solve the problem! The problem is clear! |
4/13/2009 8:47 AM | |
Posts: 2661 Rating: (279)
|
Ok. |