Industry Online Support
Technical Forum
6/1/2012 1:56 PM | |
Posts: 2 Rating: (0) |
Hello everybody, I have been finding this thread before but I have not find yet the solution. I have WinCC flexible 2008 SP1 and if I make a simple change in a faceplate it doesn't update in all the instances that I have. I have tried: /tf/WW/en/Posts/47854 * Options --> Delete Temporary Files" and after this "Project --> Compiler --> Generate". * /tf/WW/en/Posts/54437 1. Options > Delete temp files, then Rebuild All 2. File > Save and Optimize - Archive before you do this. I had it "optimize" my MP277 out of the project, as in, it disappeared 3. Step 7 > Save project With Reorganization 4. Right click > reset Instance Data (not explained in help so I'm not sure exactly what this does) 5. As a very last resort, right click on Flex icon in tray at bottom right and do a reset, which resets all your preferences to defaults. It didn't work for the guy I was helping. Anything of this worked for me, , any idea? |
Last edited by: itbcn at: 6/4/2012 11:47 AMHello everybody, I''ve been doing some test, and what is working better for me it''s "4. Right click > reset Instance Data ". I recommend to use it, although I haven''t found any documentation about it. Bests regards, |
|
6/5/2012 4:53 PM | |
Posts: 3037 Rating: (192)
|
Hello, I have check it with WinCC flexible 2008 SP2 update 13. The update of faceplate in thescreens works. Service Pack 2 for WinCC flexible 2008 Update for WinCC flexible 2008 Service Pack 2 Tweety |
6/13/2012 9:17 AM | |
Posts: 2 Rating: (0) |
Hello Tweety!! Thank you very much!, it totally worked!. Moltes gràcies. |