4/2/2013 1:33 PM | |
Joined: 5/18/2006 Last visit: 10/21/2020 Posts: 170 Rating: (63) |
The only difference between the block icons on the @PCS7Typicals*.pdl (where the auto generated icons come from) and the @Template.pdl (mentioned by mark1507above) is in the Type property. In the @Template.pdl the block icons have the leading '@' symbol removed from the Type property. So another method is to lay down the standard @PCS7Typicals*.pdl icon (or better yet copy/paste an existing tagged icon). Select the copied icon and change the Type property as described above. Can do this in bulk if you have already laid a bunch of these copied icons down on a graphic. This can be doneby selecting all copied icons and then selecting Linking/Text from the edit or context menu. Within the Linking/Text dialog can do a search/replace to change the Type property as required. cabreytj |
Follow us on