5/26/2011 10:54 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hi all, Is for calculations in the LOGO! with the block "analog amplifier" a dezimal factor GAIN_x necessary and is the value out of the specification, then you can use two (or where appropriate also more) blocks "analog amplifier" in series with the here calculated factors a and b for the parameters GAIN of these (two) analog amplifier. The parameter "offset" of the 1st analog amplifier should always = 0 and that of the 2nd according to the requirements being defined to the use. Is the amount of the the decimal factor's GAIN_x > 100, then we use a 3rd analog amplifier before the both other with an integer value for the parameter GAIN_0. Attachmentfactorization_tool_LOGO.zip (184 Downloads) |
==> Meine TAG-Listen: "deut." |
|
4/23/2012 6:02 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hello, are this tool helpfull to you to program the LOGO! - please tell me your point of view. Best regards Betel |
==> Meine TAG-Listen: "deut." |
|
Follow us on