7/22/2020 8:50 AM | |
Joined: 4/28/2015 Last visit: 7/24/2024 Posts: 27 Rating: (1) |
The panel has now been Factory Reset but there was a few hurdels. You need to donwload the Firmware Package for the Unified Panels: https://support.industry.siemens.com/cs/ww/de/view/109746530 Then you should be able to follow the manual to do a factory reset. But in my case the panel had no IP address when it booted in maintanance mode. You can't set the IP address from TIA portal, so you need Siamtic Manager to set the IP address: https://support.industry.siemens.com/cs/ww/en/view/109773842 Before you try setting the IP address make sure the PG/PC interface is configured with the right interace. |
Last edited by: JanMagne at: 07/22/2020 08:51:10Last edited by: Jen_Moderator at: 07/22/2020 11:03:13Optimized links. |
|
This contribution was helpful to2 thankful Users |