10/12/2009 8:21 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, Do you have another Siemens software installed in PC? What about bmp screen shot with error? Regards |
10/14/2009 2:41 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, did you read this FAQ -> http://support.automation.siemens.com/WW/view/en/29420407 Your FAQ ID i can not found. With the log File, i mean, only people from the siemens Hotline cando something with this file. regards, |
10/23/2009 12:17 AM | |
Posts: 5 Rating: (2) |
Hi walter_g, What operating system are you working on? I just worked with a client to install WinCC Flex 2008 on Windows XP SP3 which was having failed Microsoft SQL Installation errors. Here is what we had to do to work it out. SQL failed at two points, the VSS Writer and the MSXML 6.0 failed as well. This is a known Microsoft issue and the work arounds are as follows: 1. Use the Microsoft cleanup tool to remove entires tied to MSXML 6.0, this will take care of that issue. http://support.microsoft.com/kb/968749 2. Open Control Panel -> Add/Remove Programs. Uninstall VSS Writer and then use the clean up tool from #1 to remove any additional entries to VSS Writer. With that done our MS SQL Server 2005 installed and configured no problem. Now we are having some sort of issue getting theSP1 installedfor flexible. Nic |
Follow us on