1/27/2017 10:05 AM | |
Posts: 4 Rating: (0) |
I use Failsafe DO with CPU 414-4H but when I download my program to CPU , SF led of F-Do go to red state. I think an error occure in Failsafe DO you Can see Diagnostic Buffer of F-DO Module Bellow: Order No./ Description Component Version Event 1 of 3: Event ID 16# F980:8031 Event 2 of 3: Event ID 16# F980:0201
------------------------------------------------------------------------------------------ |
Last edited by: Girigopal at: 1/27/2017 10:07:36 AMLast edited by: Min_Moderator at: 1/27/2017 2:03:20 PMNew subject after splitting |
|
1/27/2017 10:09 AM | |
Posts: 4 Rating: (0) |
I cannot able to see the reply can you please send me... |
1/27/2017 11:03 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi, have you set the DIP-Switches of the 6ES7 326-2BF01-0AB0? Have a look in the manual, chapter 4, how to assign the F-destination-address. SIMATIC Automation System S7-300 ET 200M Distributed I/O Device Fail-safe signal modules hope this helps, regards, |
FCK WAR! |
|
1/27/2017 12:18 PM | |
Posts: 4 Rating: (0) |
Yeah the DIP switch setting are the same as per hardware config. But still I am getting PASS_OUT and QBAD as 1 in CH_DO. Please help to resolve the same. |
1/27/2017 6:03 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (77) |
Hi Girigopal, Can u share HW config.? I would like to know monitoring time parameters and all available I/Os. If more safe I/Os are there, u need to increase monitoring time for profisafe frame. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
1/28/2017 4:34 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (77) |
Hi Girigopal, It's great feeling that my suggestion has helped you. Check everything for de-passivated channel. Connect healthy sensor to it. Check driver connections whether proper symbol is connected. Better to delete it and add new driver block & compile it. Another suggestion is to initially not to use acknowledge command and let reintegration be automatic. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on