8/5/2013 3:23 PM | |
Joined: 8/5/2013 Last visit: 8/9/2013 Posts: 2 Rating:
|
Hello! I need some answers and solutions. We have a farm (no internet connection) and we allready have automation for lights and food lines. Now we want to control this with mobil phone (everywhere) and at my home (internet connection). I allready buy a communication module cp 1242-7. Im still amater in plc programming so i need some help J . We only have tags with BOOL type... So now i want do this: MOBIL PHONE · when i send from mobilphone to CPU sms with text »light1=on« then should light1 turn on or same for light1=off · if CPU is without power then send sms from CPU to mobil phone with text »alarm no power« · if for example m0.0 is false then send sms from CPU to mobil phone with text » line1 alarm« COMPUTER I want monitor and modify values with computer at my home(webserver or something). I allready see project examples (https://support.automation.siemens.com/WW/llisapi.dll?query=set+value+sms&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx&lang=en&siteid=cseus&objaction=cssearch&searchinprim=0&nodeid0=45605894) , but i dont know how to put my project and this project together. I know this is 30 minute task, but i dont understand this examples.. Can anybody help me? J i attach a picture... |
8/5/2013 4:02 PM | |
Joined: 7/7/2010 Last visit: 12/9/2019 Posts: 8266 Rating:
|
Couple of no PLC code ways to accomplish it without needing to work with the SMS side of things for the "from mobile phone to plc" parts. There is the built-in web server you can use to monitor using your mobile phone (via farm wifi if it reaches), and the s7-1200 app (iphone/android), plus the web server when at your farm's central computer. As for actually setting up the sms on the plc, there is some sample code on these forums. The search box is having problems, so I tried google. It came up with a link but the support site is having problems. If it works, this is the FAQit found: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=58638283&nodeid4=20229805&nodeid0=42782043&load=content&lang=en&siteid=cseus&aktprim=4&objaction=csview&extranet=standard&viewreg=WW |
science guy |
|
Follow us on