9/13/2018 11:36 AM | |
Joined: 10/7/2009 Last visit: 8/19/2023 Posts: 266 Rating: (92) |
Hi, |
This contribution was helpful to1 thankful Users |
9/13/2018 11:54 AM | |
Posts: 2826 Rating: (684) |
Less on topic, but worth as an application sample: https://support.industry.siemens.com/cs/ww/en/view/27864874 |
This contribution was helpful to1 thankful Users |
9/13/2018 3:23 PM | |
Joined: 3/13/2018 Last visit: 5/20/2022 Posts: 57 Rating: (0) |
Thank you for all your answers. But now i am faced with another problem. Since the encoder is connected to I0.0 input of the controller, i assumed that HSC0 counter must be implemented in the controller program. But for some reason the program doesn't implement HSC0, it also doesn't use input I0.0. But it calculates the length in VD44 from input I0.0(it tested in practice). I cannot understand how this can happen. I would be grateful for any assumptions. The program code is attached. Sincerly, thank you for your help. AttachmentDrateks original.zip (170 Downloads) |