5/30/2014 1:59 PM | |
Joined: 10/29/2012 Last visit: 9/12/2024 Posts: 102 Rating: (1) |
Dear users, Thank you all in advance.
|
5/30/2014 2:14 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Fault tolerance is not suported. |
This contribution was helpful to1 thankful Users |
5/30/2014 2:59 PM | |
Posts: 510 Rating: (117) |
However the 400H is not supported in TIA Portal. It must be programmed with Step7 V5.x. Regards, billwest |
This contribution was helpful to1 thankful Users |
5/31/2014 10:51 PM | |
Posts: 8946 Rating: (999) |
Not yet, but it will be sooner or later. |
6/1/2014 10:29 PM | |
Joined: 7/2/2008 Last visit: 8/26/2024 Posts: 928 Rating: (308) |
DearIBN-Service, Is this some kind of real informationor some kind of vision/hunch? All i can see at this moment is contradicting to the assumption of new 1500 fault tolerant CPUs. - SIMATIC Manager STEP7 is going to be killed by the TIA. - However, SIMATIC PCS7 is going to continue as a software but withsome kind of different CPU with different CPU architecture/processors(1st time to see 450MHz multiprocessor). -Even the new CPU 410-5 will not be programmed by SIMATIC Manager or TIA (Only PCS7). . -Siemens has been striving to change customer's opinions in PCS7 as not a true DCS since it is based on a PLC ( which is 100% stupid/wrong). -Siemens promotes 410-5 as an exclusive controller for DCS systems. -I've been asking every Siemens guy I met why the TIA doesn't support H system and the answer was always PCS7 is the solution fortruefault tolerant systems. -So, I don't think we will see an 1500 competitor to the new 410-5H although I wish so. You know fault tolerant CPUs are not WinCC (i.e a new version every couple of months). I hope I'm wrong and if you have real information "not rumors" then I will be the ever happiest. Best regards, H-H
|
This contribution was helpful to2 thankful Users |
Follow us on