6/22/2013 3:15 PM | |
Posts: 378 Rating: (73) |
Dear All, I have a problem on my AO4X12Bit (6ES7 332-5HD01-0ABA0) module, for controlling SSR. 1. There is RED LED on SF. 2. Here is online dignostic information: External error Faulty module No external auxiliary voltage Parameters have not been assigned to the module. I have attached here my HW configuration, I have checked every wiring and powersupply and replaced the module but still the problem not solved. Any help? Rgs AttachmentHWConfig.zip (280 Downloads) |
6/22/2013 4:23 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, Is the 24V at the module, measure between pin 1 and 20. What type of output you use? In case of V output don't forget the bridge between QVx and SOx pin 3 and 4 for channel 0. Did you setup the module right, another printscreen of the module setup could help us. Did you download the hardware config? And note: If you reassign parameters in RUN, the following special characteristic applies. SF LED is lit: If a diagnostics was pending prior to reconfiguration, the SF LEDs (on CPU, IM or module) may be lit even though diagnostics is no longer pending and the module is operating correctly. Solution: ● Only assign new parameters if no diagnostics is pending, or ● unplug module and plug it in again. Check all again in the manual Regards, Marcjan |
Problem solved? |
|
6/22/2013 4:48 PM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
Hidesmul24 Fast tips to solve your problem: 1) The voltage supply of the module is missing. Check the voltage on the pins or check the feeding fuse might blown 2) the Parameters of the module should be reassigned and unplug then replug the module again after downloading the configuration 3) if all the previous does not fix your problem in addition to whatMarcjanmetioned before try to replace the module by a new one |
Best Regards |
|
6/22/2013 7:47 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Hello, I have highly doubt on posibility 1 so double check it. |
VANDE MATARAM..... |
|
6/26/2013 7:39 PM | |
Posts: 93 Rating: (13) |
Dear desmul24, In your programm all outputs on that cardare occupied? or only SSR output is used and all other are spare?? |
Follow us on