9/13/2012 7:46 PM | |
Joined: 10/31/2006 Last visit: 4/20/2024 Posts: 26 Rating: (0) |
In attachment you may see details of FB who is not green in OB1. He is very simple and short. Best regards Attachmentfb.pdf (207 Downloads) |
9/13/2012 7:59 PM | |
Joined: 7/7/2010 Last visit: 5/9/2024 Posts: 14701 Rating: (2356)
|
In this thread, I helped someone with a similar problem: /tf/WW/en/Posts/70875 As simple as the logic is, my guess is your DBs are not set up with absolute addressing, or your outputs are not 752/754 or your inputs are not 124/126. I notice also there is T3 & T4. What is T3/T4? If it is a timer, should it be T3.Q & T4.Q? Something is out of range or unavailable. The diagnostic buffer should show something about the problem. If the DBs are symbolic, you will need to delete and recreate them. I think you can select all / copy the details, create the new db with absolute references (compatible with s7-300/400 mode), and paste. |
science guy |
|
Follow us on