Industry Online Support
Technical Forum
2/18/2009 12:50 PM | |
Posts: 37 Rating: (0) |
As per the attached ET200M manual,i am doing timestamping outside of S7400 CPU. |
2/19/2009 12:46 PM | |
Posts: 37 Rating: (0) |
Actually, there are two ways of selecting ET200M from the NCM/PC manager hardware catalogue. 1. From "Additional Field Devices" as shown on Project.jpg 2. From "ET200M" section. as shown in ET200M.jpg (The attachments are attached along) In both the cases, we have an option of choosing time synch. interval. So, which out of the twoshould bean appropriate method of configuring ET200M for timestamping.? AttachmentAttachments.zip (170 Downloads) |
2/19/2009 1:55 PM | |
Posts: 2348 Rating: (263) |
I used second (Et200M.jpg). Created test project, inserted 321-7BH01 there - timestamp tab is active |
2/20/2009 4:05 AM | |
Posts: 37 Rating: (0) |
But the tab is active even if we choose the ET200M from "Additional Field Devices" after installing the appropriate gsd file. |
2/20/2009 8:37 AM | |
Posts: 2348 Rating: (263) |
Could you share with us how did you managed interrupts from ET200M with CP? |
Follow us on