8/23/2014 4:35 AM | |
Joined: 7/30/2014 Last visit: 2/1/2024 Posts: 9 Rating: (0) |
Hi Georgio , i've study the block diagram and it looks normal, regarding the motor time i still have no clue about how to set it and i just left it default. yet the intergration time is just a TI setting? About the gain for the control error, i suspecting that my setting for gain is too low, and the intergration side is too high then it covers the Propotional Gain's effec + the disturbance value, i can't see any linear effect from PV,SP side. I've uploaded the PID blocks of mine, please help me check it when you have time.... Really appreciate your help... Alan
Attachmentpid_test.zip (154 Downloads) |
Alan |
|
8/23/2014 1:29 PM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359)
|
Hello, First you should ensure that type of process and actuator are suitable with control strategy supported by FB42! The uploaded project is not a complete version your works as it doesn't contain a minimum of parameters to be considered and available while calling FB42.Read THIS topic from the German conference on some crucial issues to be dealt with.Also consider the following hints:
More to read in Controlling with SIMATIC (or the newer german version) I hope this helps, Hamid Hosseini |
This contribution was helpful to4 thankful Users |
Follow us on