3/17/2017 2:07 PM | |
Posts: 16 Rating: (1) |
I need program with fifo that remember which one of 3 digital inputs had become active during the time .When input is active it activate corresponding digital output, when I1 drop to "0" Q1 is also "0". Only one output may be active, others is memorized in fifo array. When inputs goes to "0" in same way they was memorized in "FIFO array" everything is OK, problem is when it memory eg.sequence I2-I3-I1 and during Q2 is active, I3 drop to "0". My program is based on modified program from this link: https://support.industry.siemens.com/tf/ww/de/posts/immer-nur-einer-von-10-ausg-ngen-gleichzeitig-schalten/158723?page=2&pageSize=10 AttachmentFIFO3 siemens forum.zip (281 Downloads) |
Follow us on