12/1/2014 3:46 PM | |
Posts: 6 Rating:
|
Hi I am using the Simatic S7-1200 1212C AC/DC/RLY with the TIA V12 I am trying to create a user defined webpage but seem to be unable to find the global library AT_User_Defined_webpage_2012 required to tie the virtual logic in with the actual logic. I can`t seem to find the Global library that are shown in siemens video tutorials in respect to LINK:https://www.youtube.com/watch?v=o8dqSkLWQWo Can any one tell me where I can find such global library's? As the only libraries I have are shown in : (See screen shot) Also where can I find additional global library’s such as: AT-1_Simple_Movements_2012_LIB and WinAC_MP. Could you also please give me instructions on once a global library is created, taking that created global library and tying it into the tags in a current project. AttachmentUSER DEFINED WEB PAGE (FINDING GLOBAL VARIBLES1).pdf (216 Downloads) |
Last edited by: KMcD at: 12/1/2014 4:38 PM |
|
12/2/2014 2:38 PM | |
Joined: 7/7/2010 Last visit: 3/2/2021 Posts: 10196 Rating:
|
Maybe this thread will help: /tf/WW/en/Posts/85074 |
science guy |
|
12/3/2014 5:08 PM | |
Posts: 6 Rating:
|
Hihuggy_d1 Thanks for the link there looks like there is some useful code there. When I first attempted the webpage project I think a global libraries was present to tie in the actual logic with virtual logic. I think I managed to take the project global tags in form the global library then inserted them into plc tags. Then the AWP associated tags appeared in the detail view bottom LHS so they could then be tied into the project. But for the life of me I can`t remember how I did it? though it might of been deleted, but checked on another computer which has TIA V12 untouched there still just has the same basic global libraries. Basically all I want to do is to be able to operate a stop start sealing circuit via a web page. Kind of thinking there`s an easy option that I'm missing here? Any ideas? Cheers KMcD |
Follow us on