12/23/2018 5:00 PM | |
Posts: 2826 Rating: (684) |
+ Could you show a connection diagram of you plan? + How many MHz frequency is required? |
12/24/2018 11:22 PM | |
Joined: 7/5/2017 Last visit: 4/28/2024 Posts: 232 Rating: (17) |
Dear experts, Please refer attached images of rectifier circuit. Thyristor is controlling income voltage 230-440 Vac. 51-54 are gate trigger pulses. Output off T1 is 5 vdc by consider V drop rectifier diodes. Which is not shown here attached curcuit old we are modifies it to IGBT Input & rectifier diodes output. 41-42 get mV as per actual DC current flow. R1 -Y1 are 440Vac. Frequency is 10-50Hz only Regards Ramesh S Attachmentimage rectifier.pdf (91 Downloads) |
Last edited by: Ramesh S at: 12/24/2018 11:24:43 PMRaman |
|
Follow us on