6/9/2015 7:00 AM | |
Posts: 5225 Rating: (1184) |
Hi. Where to would you wish to update to and why? You cannot update FW3.0 to anything worth while. Greetings. |
This contribution was helpful to1 thankful Users |
6/9/2015 7:15 AM | |
Posts: 10 Rating: (0) |
sir, kindly can i know which all are the s7 1214c dc/dc/rly PORT NUMBER - 6ES7- 214-IHG31-0XB0 available firmwares ? regards, varghese n |
Last edited by: Min_Moderator at: 6/9/2015 3:03:40 PMChange formatting |
|
6/10/2015 8:24 AM | |
Posts: 5225 Rating: (1184) |
Vargese, You have received this information from other friends already: Let me explain.. You have x3 hardware "islands" - You cannot jump (forward) between the "islands". Example FW2.0 PLC can be updated to FW2.2, but then it reaches its group's ceiling. In your case the change for FW3.0 is so small, it is not worth the effort. With all firmware updates, you have a reason to update to another firmware version: "I want to update my PLC to firmware version xxx to get the functionality of xxxx." If there is no such reason, then it is not worth doing the update. Are you and I now on the same page? |
This contribution was helpful to1 thankful Users |
Follow us on