Industry Online Support
Technical Forum
12/23/2013 11:48 AM | |
Posts: 76 Rating: (1) |
Hello, I have a PLC S71212C DC/DC/DC (6ES7-212-1AE31-0XB0). I am programing it in TIA V12. I can connect to the PLC without any problems. But when I try to download to the CPU i get message saying: "Module "PLC_1" has an invalid firmware version". I looked at the CPU to see which firmware version is but I couldn't find the number. Another problem is when I add my device (CPU) the only firmware version is 3.0 and I can't change it. Can someone please tell me how to solve this problem. In the attachment is the picture of the error. Best regards Lesko AttachmentFirmware_problem.zip (136 Downloads) |
12/23/2013 12:48 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
Hello, It looks like you have a memory card inserted that was used for other CPU. Remove memory card and try again. Using memory cards Regards, Marcjan |
Problem solved? |
|
Follow us on