9/11/2008 5:58 AM | |
Posts: 487 Rating: (36) |
Hi You transfer the license using ALM software ( automation license manager) to and from the PC/floppy. Its possible that the license was on the laptop when it crashed .In this case you can email or phone siemens and with the yellow or red floppy disk and ALM started up they will help you to get a new license) There is a procedure to follow They will check the number on the follopy and ask you to generate a number and they will give you another number to input and you license should be back. Info ( supply then the KHE nr on floppy and contact phone)
Europe/Africa Siemens AG A&D AS CS1 Autorisierung Gleiwitzer Str. 555 D-90475 Nürnberg-M Telefon:+49(0)911 895-7200 Fax: +49(0)911 895-7201
America Siemens E&A Autom. Technical Services 3000 Bill Garland Road Johnson City, TN 37605 USA Telefon: +1 423 461-2522 Fax: +1 423 461-2289 simatic.hotline@sea.siemens.com Asia/AustraliaSiemens SAE Ltd. SIMATIC Hotline 2 Kallang Sector Singapore 349277 Telefon: +65 740-7000 Fax: +65 740-7001 simatic.hotline@sae.siemens.com.sg |
Last edited by: aikona at: 9/11/2008 6:03 AM |
|
9/11/2008 4:52 PM | |
Posts: 487 Rating: (45) |
Basically, your license came on the floppy, but it has to transfered to a PC Hard disk to use it. But Floating license also allows you to install license on network. Check this link.
As described by Aikona, the license might have been on the laptop that crashed. And use tecch support to get replacement license. http://support.automation.siemens.com/WW/view/en/23322349
There are many ways to do this. via network, USB stick etc. See the link below http://support.automation.siemens.com/WW/view/en/23173081
You can not copy Siemens license. It is also illegal even if you find a way to do this. But you can movethe license from one PC to anothe using Automation License Manager. This can be done over network, Siemens floppy or USB drive - If yes, where can I find the installed licence??? Use ALM. Hereis some helpful info. http://support.automation.siemens.com/WW/view/en/22815988 |
Follow us on