11/10/2020 11:46 AM | |||||||||||||
Posts: 9 Rating: (0) |
This is the flow in json: [snip] Attachmentfiles.zip (249 Downloads) |
||||||||||||
Last edited by: slcr at: 11/10/2020 11:50:35Last edited by: Jen_Moderator at: 11/11/2020 05:36:57Added flow and image as zip file. |
|||||||||||||
11/10/2020 3:27 PM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi, I have never faced this issue nor heard about it. I don't know if this could be related to the global class definition, I have never used that to be honest. I used your flow without this definition and rebooted some times, without any problems. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
11/23/2020 10:16 AM | |
Posts: 1 Rating: (0) |
Hello there, I am the customer whose @slcr is talking about. The "settings.js" is a NodeRED configuration file and must be located at NodeRED working directory, in this case it was at /home/root/.node-red. This file is loaded when NodeRED starts and if it fails then NodeRED webserver is not loaded at all. Therefore, I don't think this is the source of the problem because the NodeRED webserver was properly loading and the global class was working like a charm. Furthermore, if any problem is found at "settings.js" it is reported to "node-red.log" file and, if you check that, it's not the case. Thanks. |
11/23/2020 2:42 PM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi, ok, this is the right settings.js file. There is another on the /usr/lib directory of node-red. Since I cannot reproduce this issue and have never seen it before I'd recommend to reach out to the node-red forum, maybe there somebody has an idea. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on