6/13/2011 8:17 PM | |
Posts: 53 Rating: (2) |
Hello, I have a Siemens positioning card FM351 and 250mm assymetrical incremental linear encoder with 2 square optput signals A*, B* and the 5V power supply. I can not make it work, It looks like the FM351 modul does not support this type of encoder . - Is it right ? - If yes, can you advice me some other encoder suitable for this modul ? Thank you very much for ANY help !!! J. |
6/17/2011 7:43 AM | |
Posts: 2348 Rating: (263)
|
Maybe you can also tell manufacturer and order num ? Just in case someone else will need it |
This contribution was helpful to1 thankful Users |
6/17/2011 2:56 PM | |
Posts: 53 Rating: (2) |
OK, the manufacturer is GIVI Misure but they dont want to sell it as a part. i've been told, that have to order the whole reading head (700$). But the part I need is very simple, there is only one 0,5$ chip (DS34C87TM) so called line driver, so I am searching the internet for some alternatives. But till now cant find anything :-( ... maybe someone could help me ? PLEASE !!!!! Thanks, J. |
Last edited by: jirimatus at: 6/17/2011 3:15 PM |
|
5/27/2014 4:41 PM | |
Posts: 29 Rating: (2) |
You can take a look at either Kuebler or Accu-Coder. |
5/28/2014 8:14 AM | |
Posts: 63 Rating: (4) |
you can try LSmecapion encoders |
9/4/2017 9:16 AM | |
Joined: 8/21/2014 Last visit: 4/24/2024 Posts: 952 Rating: (13) |
New question published by AutoGen_148962 is split to a separate thread with the subject I want to know whether a SSI signal output of a LVDT can be connected to FM351 or not?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on