5/11/2014 4:33 AM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 7/15/2008 Last visit: 1/23/2024 Posts: 382 Rating: (44) |
Hello Pauljim Well, with any Manual, ther there is a chance that there could be aprinting error. I would suggest to open aSupport Request and ask. On the other hand, are yousure nobody opend up you stopping / travering limits? and that the encoders are workingcorectly. Reagards / m.f.g |
||||||||||||||||||||||||||||||||||||||||||||||||||||||
5/12/2014 9:19 AM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||
Posts: 2 Rating: (0) |
HI m.f.g and thanks for the reply. I am not sure what you mean by "opened up your stopping/ traversing limits? I think our faults are caused by mechanical movement in our system. I just need to understand what the fault codes actually refer to so i can fully understand exactly how the system works. We have a lot of mechanical variables in our system and it only needs to be accurate to about 5 mm so once i understand better i am thinking i might be able to open up some tolerances in the servo settings to stop most of these faults occurring. Again thanks for the reply and any further help is much appreciated. Cheers Paul
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||
Last edited by: pauljm at: 5/21/2014 11:41 AMHi i can now confirm that the error is Class 04 and number 01, as per below:General data errors Error response: ”Warning” see Table 11-2 4 (04) 1 (01) Data at time of transmission unacceptable CBS or DB Cause Data not transmitted in appropriate operating mode. Effect Data not accepted. Elimina- tion Transmit data in appropriate operating mode. Hi, It usually occurs when the axis is changing from MDI to Auto. The axis stops and the SYNC bit turns to false. It also goes in to jog mode and the fault reset trigger bit turns on. The drive is still enabled, the channel is initialised and the Start enable bit is still on. Do i need to delay the transition or stop the axis when switching from MDI to Auto? MdI target position is 9000 and Auto target is 140000. Machine faulted today with target of 140000 and actual position of 9013, so it was during the transition from MDI to Auto that it faulted and stopped. Thank you for any further help. Paul |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||
Follow us on