8/10/2012 2:24 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684)
|
Hello Mortier; You show pulses giving a positive pulse at around 8 V. This does not match with the positive signal levels for the FM 350-2, as shown in this manual (and extracted in the attachment). SIMATIC S7-300 FM 350-2 Counter Module If you are stuck with using this specific equipment you wopuld have to look for some type of signal conditionner or pull-up circuit that would give you a readable signal as seen from the FM 350-2. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on