12/27/2014 4:14 PM | |
Posts: 5 Rating: (0) |
nobody to help me |
12/27/2014 7:12 PM | |
Posts: 8946 Rating: (999) |
First it may be a good idea to explain if you are talking about FM352-5 or FM350-2. Then you may explain to us, what is not clear...? |
12/27/2014 10:27 PM | |
Posts: 5 Rating: (0) |
Ok this is fm350-2 I Would like to know What is the method to configure The Encoder and fm350-2?
|
12/28/2014 8:58 AM | |
Posts: 8946 Rating: (999) |
First, you have to install the FM350-2 Software package Then you will find also the documentation of FM in the documentation folder. You can configer the FM in HW-config, but it is not possible to use an absolute encoder with FM350. |
12/28/2014 3:41 PM | |
Posts: 5 Rating: (0) |
Why? |
12/28/2014 3:52 PM | |
Joined: 9/27/2006 Last visit: 9/23/2024 Posts: 12282 Rating: (2685)
|
Hello, From the FM 350-2 manual: no absolute encoder modules mentionned. SIMATIC S7-300 FM 350-2 Counter Module The FM 350-2 can count signals generated by the encoders listed below. Only bounce-free encoders are permitted. ● 24-V incremental encoders, push-pull or current-sourcing switches ● 24-V pulse encoders with direction level ● 24-V initiators without direction level for example, light barrier or BERO (type 2) ● NAMUR encoders in accordance with DIN 19 234 One possible option could be the FM 351: FM351 for the measuring of the actual value Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 12/28/2014 3:57 PM |
|
This contribution was helpful to1 thankful Users |
12/29/2014 8:24 PM | |
Joined: 12/7/2012 Last visit: 7/30/2024 Posts: 25 Rating: (0) |
nobody to help me |
Follow us on