2/8/2015 5:52 AM | |
Joined: 6/2/2010 Last visit: 8/29/2024 Posts: 41 Rating: (0) |
Normal
0
false
false
false
EN-US
X-NONE
X-NONE
MicrosoftInternetExplorer4
Dear sir, For our machine we are using fm354 module for position control CPU s7 315 . As per fm354 manual we are made program which one is attached for your reference We used fc0 , fc1, fc2, fc3 OB1, OB100,OB86,OB40, and UDT , we are using fm354 for first time . we are not able to get reading from attached program . we are very much thankful to if you give feedback where have gone wrong. We have faced following problems while using above program. 1. While calling FC1 cyclic in OB1 main CPU get in error mode or some time all the digital output start flickering. 2. We are able to read linear scale pulses in hardware diagnostic mode while CPU in stop mode but not able to read from UDT AW-DB block. 3. Also not able to give -10v to 10v command from this module.
Please suggest how to solve the problem
Regards Ravi ShankarAttachmentprogram.zip (115 Downloads) |
2/8/2015 2:10 PM | |
Joined: 6/2/2010 Last visit: 8/29/2024 Posts: 41 Rating: (0) |
sir, i am uploading the diagnostics buffer of fm354 module in which external error is showing. In attach file error is showing external error . regards ravi shankar. AttachmentDoc1.docx (109 Downloads) |
Follow us on