Industry Online Support
Technical Forum
1/28/2011 9:43 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Basically these are the steps. However, some changes should be taken into consideration, such as the altered connector assignment (40-pin) and the incompatibility with the firmware and the basic function blocks of the previous FM. This necessitates changes in the user program and a new entry of the machine data. If NC programs are used that contain synchronous actions, the program must possibly be adapted. More information about the FM357-2 is available from the On-line Support of our Customer Support. Product Brief of the FM357-2: ID 2614071 Hristo Mihalev |
Follow us on