2/25/2019 6:43 AM | |
Joined: 3/7/2017 Last visit: 4/27/2024 Posts: 75 Rating: (0) |
Dear Expert, How is create connection between FM458-1DP with sinamic S120? Thanks |
2/25/2019 8:15 AM | |
Joined: 3/7/2017 Last visit: 4/27/2024 Posts: 75 Rating: (0) |
Do you have examples project ? |
2/25/2019 8:40 AM | |
Joined: 3/7/2017 Last visit: 4/27/2024 Posts: 75 Rating: (0) |
How about configuration in the sinamic sir? |
2/25/2019 9:01 AM | |
Joined: 8/25/2006 Last visit: 5/6/2024 Posts: 2203 Rating: (277)
|
You can use as an example project for S120+S7-300. |
2/25/2019 9:19 AM | |
Joined: 3/7/2017 Last visit: 4/27/2024 Posts: 75 Rating: (0) |
Ok thanks expert and best regard |
2/26/2019 5:48 AM | |
Joined: 3/7/2017 Last visit: 4/27/2024 Posts: 75 Rating: (0) |
Dear Expert, |
2/26/2019 5:53 AM | |
Joined: 8/25/2006 Last visit: 5/6/2024 Posts: 2203 Rating: (277)
|
Without any information it is difficult to understand where is the problem. Upload your project here. |
2/26/2019 5:54 AM | |
Joined: 3/7/2017 Last visit: 4/27/2024 Posts: 75 Rating: (0) |
Does the CF blinking LED on FM458 affect the program? |
2/26/2019 5:58 AM | |
Joined: 8/25/2006 Last visit: 5/6/2024 Posts: 2203 Rating: (277)
|
CF could affect the program and the incorrect program could also affect the CF. |
2/26/2019 6:58 AM | |
Joined: 3/7/2017 Last visit: 4/27/2024 Posts: 75 Rating: (0) |
I am send actual current from sinamic but not event in the CFC [FM458] |
2/26/2019 9:53 AM | |
Joined: 3/7/2017 Last visit: 4/27/2024 Posts: 75 Rating: (0) |
Ok expert now is running I am change lenght data on the CTV_P pin NBY olso on the DRV_P. Thanks expert..and best regard |
2/26/2019 9:54 AM | |
Joined: 3/7/2017 Last visit: 4/27/2024 Posts: 75 Rating: (0) |
Reference
AttachmentTDC set communication.pdf (356 Downloads) |
Follow us on