Industry Online Support
Technical Forum
5/15/2012 5:42 PM | |
Posts: 2 Rating: (0) |
Hello, The task of connecting the emulator of the SSI probe FM458. RS485 of emulator provides an output voltage with the difference only 2 volts. After connecting to the M458 on the line with the data appears offset from zero, which causes the logic 0 corresponds to 0 volts and a logic 1 corresponds to 2 volts. How do I get when connecting the FM ± 1 volt? http://www.wiki-kollmorgen.eu/wiki/DanMoBilder/file/pdf_archiv/drives_AC_digital/SERVOSTAR/SR300/2011-09/sr300_e.pdf This is a reference to the description of servoamplifier, which emulates the SSI encoder. On page 86 a description of the encoder emulation. Thanks. |
5/17/2012 4:53 PM | |
Posts: 2 Rating: (0) |
Thank you for reply. The problem was solved by replacing the RS485 chip on the same. topic can be closed. |