10/26/2020 10:34 AM | |
Posts: 22 Rating: (0) |
Hi! I want to be able to connect with wincc v16 via opc ua with my s7 -1200 as a server through the iot 2050 gsm / gprs modem But I am totally lost with IpTables or Nftables. I am attaching a diagram of what I want to do in case you can help me. Thanks! Best regards! AttachmentPresentación1.pdf (567 Downloads) |
10/26/2020 1:39 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, with the current example image version (V1.0.2) we have some problems with iptables. To use iptables you would need to build an image from the current master branch at github. With this image you can then install iptables. In this post you can find some information about that as well as the two commands you'll need to setup the routing. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on