8/3/2018 7:51 PM | |
Posts: 10 Rating: (0) |
This is what it looks like: |
8/6/2018 9:08 AM | |
Posts: 2930 Rating: (432)
|
Hi LADII, to create program without LOGO! Soft Comfort is possible, but not very comftable. Here some tips from my side to make your life with LOGO! easy: Tip 1: Go to Siemens LOGO! page and download the LOGO! Soft Comfort Demo version. (Even if you cannot transfer the program to LOGO! you can create the program and test with the simulation. Then you can program LOGO! Manually. Tip 2: Check if the relais for Q1 is OK. If Q1 should be ON, use a messure instrument to check if the power for the lamps directly at LOGO! Q1 is OK. Tip 3: If Q1 in your LOGO! is not OK, then you can change in your Program and replace Q1 by Q4 (if Q4 is not used). Don't forget to rewire from Q1 to Q4. Tip 4: On the Siemens LOGO! Web-page you can also find Web Based Trainings for LOGO!. Click on "Web Based Trainings". Her you can find a view WBT's Tip 5: Think aboute geting a actual LOGO! Starterkit. Here you get all you need including LOGO! 8 with user defined Web-Pages programming SW LOGO! Soft Comfort. With the WBT you can then creat an option to control your "Lights" with a smartphone. The only additional HW you need is a WiFi-Router. Tip 6: In LOGO! there is an function block called "Random Generator". You can find it in the Demo-SW at "special funktions". Once you "enable" this FB, then randomly it turns ON and OFF the FB output. With the demo SW and it's simulatin you can play and test if this FB can be used in your program. I hope this helps. |
Last edited by: Helmut_13 at: 8/6/2018 9:08:59 AMLast edited by: Helmut_13 at: 8/6/2018 9:10:41 AM |
|
This contribution was helpful to2 thankful Users |