3/9/2017 3:11 AM | |
Joined: 9/9/2015 Last visit: 9/25/2024 Posts: 727 Rating: (278) |
Hi all, Recently i encountered free text configuration issue in PCS 7 V8.2. I configured messages of free text 1 to 5. Supposingly, after i configured in AS, then by using OS compilation, the messages and free text will be able to transfer to wincc explorer and be seen in alarm logging. However, after I had done full os compilation, the free text 1 to 5 could not be compiled and transfer over to wincc explorer. Here is the solution, There is an update version of AS-OS Engineering V82 Upd2. You may request this with Siemens Support. After I update the version from AS-OS engineering to the Update 2, the issue had solved.
|
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to2 thankful Users |
3/9/2017 8:34 AM | |
Joined: 3/14/2008 Last visit: 9/25/2024 Posts: 2097 Rating: (938)
|
Hi JazTai, Thank you for your input. Last week I received notification that AS-OS Engineering V8.2 SP1 has been released. AS-OS Engineering V8.2 SP1 download Do you mean this update instead of Update2? At least SP1 is the latest version. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
3/9/2017 9:55 AM | ||||||||||
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191)
|
For PCS 7 V8.2 the following AS OS Engineering updates are released:
Source: Siemens, Compatibility Tool, http://www.siemens.com/kompatool We recommend to install the latest update, in this case AS OS Engineering V8.2 SP1. Download |
|||||||||
Last edited by: Thunderstorm at: 3/9/2017 9:56:37 AMLast edited by: Thunderstorm at: 3/9/2017 10:01:15 AMSIMATIC PCS 7 - Overview |
||||||||||
This contribution was helpful to1 thankful Users |
3/25/2017 6:54 AM | |
Joined: 9/9/2015 Last visit: 9/25/2024 Posts: 727 Rating: (278) |
My update version is AS-OS-Engineering V8.2 Upd2. Thanks for the information on the latest update. I will install the latest update later. Here attached with the pictures of my installed software. Update 2 was the software update that solved my free text configuration issue. Thank you any ways. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on